Other

Start Topic

Popular topics

Network vedio Recorder

Murali
0 Votes
Need to develop the network vedio recorder by using renesas processor....

Add a Reply

Recent Topics Replies Last Reply
fu
The LINK_PHY pin of TPS-1 is always low,why!
1 Vote
0 Reply

Category

Last Topic

    • Network vedio Recorder
    • Need to develop the network vedio recorder by using renesas processor.
    • The LINK_PHY pin of TPS-1 is always low,why!
    • Recently,I have started to use TPS-1.But I found the LINK_PHY pin is always low,and the communication between the computer and TPS-1 is interrupted,rather than say it never start communication.