RZ/G Qt User Guide
Update: October 22, 2018

Renesas Electronics Corporation
Basic information and the steps to developing applications about the open source version of Qt which is included in Verified Linux Package are described.

Product Overview

This guide describes the information about the open source version of Qt, which is included in the Linux package, and specific to the RZ/G such as the structures on the build system and the relationship between the other software in the packages. Whole steps needed from design to build are also explained.

[Target Products]
◆ Hardware
 - RZ/G Series
◆ Software
 - RZ/G Verified Linux Package [Evaluation/Product version] Kernel version 4.4-CIP