RZ/G1 Group Application Note
Update: October 22, 2018

Renesas Electronics Corporation
In this manual, we present a sample application that will be helpful for developing applications that run on the RZ / G series Linux OS and explain its contents.

Product Overview

This manual describes how to develop a sample application that runs on the RZ / G series Linux OS.
In addition to the sample application using Linux functions, sample applications using GStreamer and Qt are explained in each chapter.

Each chapter consists of two sections.
In the first section, we describe a brief application as an example, outline of the application, development environment for creating the application, source code, how to build and execute it.
In the second section, we describe the sample application for each section, and guide you on the source code, the composition of the source, how to obtain it, and the result of execution.

Once you request it from this page, you will be able to download the following from your "MyPage".
【Deliverables】
◆ Documents
 - RZ / G Series Application Note
◆ Sample source code
 - Linux application sample source code set
 - GStreamer application sample source code set
 - Qt application sample source code set

【Target Products】
◆ Hardware
 - RZ/G Series
◆ Software
 - RZ/G Verified Linux Package [Evaluation/Product version] Kernel version 3.10-LTSI
 - RZ/G Verified Linux Package [Evaluation/Product version] Kernel version 4.4-CIP
 - RZ/G Multimedia Package [Evaluation/Product version] Kernel version 3.10-LTSI
 - RZ/G Multimedia Package [Evaluation/Product version] Kernel version 4.4-CIP

Note) From the revision 1.04 issued in Oct. 22, 2018, descriptions are added for new environment of Verified Linux Package issued in the same day.