User Profile

Start Topic
PrinceFree

PrinceFree

  • Posted Calibrating low speed on chip oscillator to Community
    It a low power application which requires the micro to be in STOP mode 99.85% of the time. I want to use the fIL (low speed on chip oscillator: 15K=kHz +/- 15%), to generate periodic interrupts every 500msec. Timer RJ...
Subscribe to feed Recent Actions from PrinceFree